Use the Network Browser to Go Online with the Controller

To go online with the controller, you must first specify a communication path in the
Studio 5000 Logix Designer®
application.
  1. Open or create a Logix Designer application project.
  2. In the application, click the Network Browser.
    This image shows an example of the Network Browser in Logix Designer.
  3. Expand the communication path and select the controller.
  4. To store the path in the project file, click Set Project Path.
    TIP:
    If you store the project path in the project, then you do not have to choose the path each time you go online.
  5. After choosing the communication path, click Go Online.
    This image shows where to click to go online in Logix Designer for a ControlLogix 5590 controller.
    Go Online uses the highlighted node in the tree, regardless of the setting for Path in Project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal