Use a Recent Communication Path to Go Online with the Controller

You can also select a recent communications path and go online or apply it to your project.
  1. In the application, click the arrow that is on the Path bar.
  2. On the Select Recent Communications Path dialog box, choose the path.
  3. To store the path in your project, click Set Project Path.
  4. Click Go Online.
    This image shows how to select a recent communication path in Logix Designer.
  5. Once you establish a communication path, you can choose Go Online from the Controller Status menu.
    This image shows where to change the controller status in Logix Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal