Insert/Append Mode command
Choose this command to switch from the Insert mode to Append mode, and vice versa.
TIP:
Whether a language element is inserted or appended depends on the insert state of the editor. (The current state appears in the status bar (APP or INS).) Pressing Ctrl + I allows you to toggle between Insert and Append modes. The default mode is Insert mode.
Provide Feedback