AC Line page
Use the settings on the
AC Line
page to configure the AC Input properties for a regenerative converter.
TIP:
Top open the AC Line page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickGeneral.
- In theAxis Configurationbox, selectRegenerative AC/DC ConverterorLow Harmonic AC/DC Converter.
- InCategories, clickAC Line.
Use the settings to:
- Configure the AC line voltage applied to the converter.
- Select whether the converter input power to the AC line is single-phase or three-phase.
- Select the nominal frequency of the AC line connected to the converter.
- Select which AC Line source is active for the converter.
- Set the power rating of the AC line source and alternate AC line source.
- Set the impedance of the AC line source and the alternate AC line source as a percent of the impedance rating.
The
AC Line
page is available when, on the General
page, the Axis Configuration
is set to Regenerative AC/DC Converter
or Low Harmonic AC/DC Converter
.The parameters are unavailable when in online mode and when the axis is
Servo On
.Parameter | Description |
|---|---|
Converter AC Input Voltage | Specifies the AC line voltage during normal operation. The default is 480 Volts (RMS) |
Converter AC Input Frequency | Specifies the nominal frequency of the AC line connected to the converter. The available values are:
|
Converter AC Input Phasing | Specifies whether the converter input power to the AC line is single-phase or three-phase. The available values are:
|
Source Select | Determines the AC Line source that is active for the converter and applies the configured impedance and power rating to the converter. The available values are:
|
Source Power | Specifies the power rating (kVa) of the transformer or generator feeding power to the converter as a percentage of the converter's power rating. |
Source Impedance | Specifies the impedance of the AC Line source as a percentage of the transformer or generator impedance rating. Enter a value 0 to 100. |
Alternate Source Power | Specifies the power rating (kVa) of the alternate transformer or generator feeding power to the converter as a percentage of the converter's power rating. |
Alternate Source Impedance | Specifies the impedance of the alternate AC Line source as a percentage of the transformer or generator impedance rating. Enter a value 0 to 100. |
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.
TIP:
The
Parameter List page may contain more
attributes than the associated page. In some cases, attributes that display on the
Parameter List page do not display on the associated page.Master Axis Parameters page to configure additional AC Line parameters. |
Provide Feedback