Error - Imported content in project may not match content in controller

Be aware that proceeding with the import, may require a full download to the controller in order to get back online.
If importing content after the
Logix Designer
application loses communication with the controller, the contents of the project may be different from the contents of the controller. Download the project to the controller in order to make sure that the content in the project matches the content in the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal