Couldn't modify final name
There is a problem setting the
Final Name
. The message may indicate one of these conditions.The Final Name is invalid
The
Final Name
entered does not follow the IEC-61131 Name Standard. The IEC-61131 Name Standard is an identifier that is a string of letters, digits, and underline characters that begin with a letter or underline character. Underlines are significant in identifiers (for example, A_BCD is interpreted differently than AB_CD). Multiple leading or multiple (consecutive) embedded underlines are not allowed, trailing underlines are not allowed, and letter case is not considered significant. (The names are composed per IEC-61131, section 2.1.2.)
TIP:
In
Logix Designer
, most component names are limited in length to 40 characters or less.Reenter the
Final Name
using the format defined by the standard or press ESC to cancel the editing mode.The Final Name creates a scope conflict for a tag reference
The
Final Name change
created a conflict between a tag in the current scope and a tag at another scope. This causes a logic change due to rebinding. Determine the conflict between the tags and resolve it.The Final Name collides with a Final Name of another object
The
Final Name
is the same as the Final Name
of another object of the same type in this import. Reenter the Final Name
using a unique name or press ESC to cancel the editing mode.Provide Feedback