Coordinate System Properties - Dynamics

Use the settings on the
Dynamics
tab in the
Coordinate System Properties
dialog box to enter Vector, Actual and Command Position Tolerance, and Orientation values for a Cartesian coordinate system.
The
Dynamics
tab is only available when configuring a Cartesian coordinate system.
TIP: To open the Dynamics tab:
  1. In the
    Controller Organizer
    , expand the
    Motion Group
    folder, and double-click the coordinate system.
  2. On the
    Coordinate System Properties
    dialog box, on the
    General
    tab, select
    Cartesian
    as the
    Type
    .
  3. Click the
    Dynamics
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal