Unable to connect from a FactoryTalk Linx OPC UA Connector to an OPC UA Server
Possible cause and solution:
- TheFactoryTalk LinxOPCUA Connector orOPCUA Server does not have network connectivity.Verify network continuity between theFactoryTalk LinxOPCUA Connector workstation andOPCUA Server.
- TheOPCUA Server software is no longer running, has crashed, or its host computer is shut down or restarting.Verify the host PC is running. UseWindowsServices to determine if theOPCUA Server software is operating normally.
- TheOPCUA Server hostname or port is incorrect.Verify the hostname and port number are entered correctly in.FactoryTalk LinxOPCUA Connector >OPCUA Servers > Endpoint URLThe path must be in the formatopc.tcp://hostname_or_ip:port/Endpoint/Namewherehostname_or_ip,port, and/Endpoint/Nameare replaced with the hostname or IP address, port number, and endpoint name of anOPCUA Server and its local discovery service. If no port is specified, theFactoryTalk LinxOPCUA Connector will attempt to connect to port 4880.
- TheOPCUA Server hostname is not resolved.Enter an IP address inEndpoint URLinstead of a hostname.
- The network hosting theFactoryTalk LinxOPCUA Connector andOPCUA Server does not support IPv4 connectivity.Ensure theFactoryTalk LinxOPCConnector andOPCUA Server connect over an IPv4 only network.
- Windowsfirewall or another software firewall is not configured to allowOPCUA Server communications.If the machine hosting theOPCUA Server usesWindowsFirewall, useWindowsControl Panel to permit theOPCUA Server to listen on the specified IP address and port number.If the machine hosting theOPCUA Server uses another software firewall, use the configuration utility included with the firewall to permit theOPCUA Server to listen on the specified IP address and port number.
- TheFactoryTalk LinxOPCUA Connector certificate has expiredRegenerate or replace theFactoryTalk LinxOPCUA Connector certificate with a valid certificate. Then, in theOPCUA Server software, locate and accept the security certificate provided by theFactoryTalk LinxOPCUA Connector.
- TheFactoryTalk LinxOPCUA Connector certificate is not trusted by theOPCUA ServerIn theOPCUA Server software, locate and accept the certificate provided by theFactoryTalk LinxOPCUA Connector.
Provide Feedback