I cannot switch between primary and secondary servers
Possible cause and solution:
- Access to the manual server switchover operation is denied to your user account, the group account to which your user account belongs, your computer account or the group account to which your computer account belongs.Update theManual server switchoverpolicy setting:InExplorer, expand theSystem > Policies > System Policiesfolders. OpenUser Rights Assignment.
- UnderManage Servers, next toManual server switchover, selectConfigure Security.
- Review the list of user and groups that have access or that are denied access.
- If a user or group has been denied incorrectly, selectAllow.
- SelectAddand add any accounts or groups that need to be able to perform a server switchover.
- When finished, selectOK.IMPORTANT:Security settings are completely separate in the Network Directory and Local Directory. Changes made to the security settings in the Network Directory do not affect the Local Directory and vice versa. If using both a Network and a Local directory, set up security in each directory separately.
Provide Feedback