The directory is in read-only mode

Possible cause and solution:
  • Your computer cannot communicate with the
    FactoryTalk
    network directory server, or if the network connection is lost while configuring the directory.
    Check the connection status of the
    FactoryTalk
    Network Directory server.
    Go to
    Rockwell Software > FactoryTalk Tools
    and run
    Specify FactoryTalk Directory Location
    . Use this tool to select the name of the computer running the
    FactoryTalk
    network directory server, or to check its connection status.
    Once you have made sure both your computer and the
    FactoryTalk
    network directory server are connected to the network, run the
    FactoryTalk Directory
    Configuration wizard again.
This error applies to only the
FactoryTalk
network directory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal