I need to revert to an earlier version of a directory
Whenever you run the wizard to reconfigure the
FactoryTalk
network directory or FactoryTalk
local directory, the wizard backs up the original directory to a file located in C:\ProgramData\Rockwell\RNAServer\Backups
. The backup files are named:- NetworkInstall*.bak
- LocalInstall*.bak
The location of the backup files is also logged to
FactoryTalk Diagnostics
. You can view the diagnostic log files using the FactoryTalk Diagnostics
Viewer.Provide Feedback