The FactoryTalk Directory Configuration wizard doesn't allow me to do something
The
FactoryTalk Directory
Configuration wizard automatically detects faults with the configuration of the FactoryTalk Directory
, and then displays the appropriate options.For example, the wizard allows you to reset an expired password to a
FactoryTalk
administrator account only if the directory actually contains an administrator account with an expired password.If you find that you cannot do something you were expecting to be able to do, try one of the following:
- In theFactoryTalk DirectoryConfiguration Wizard, selectCancel, run the wizard again, and then be sure to select the correctFactoryTalk Directoryon the opening screen.
- If another user has an account that is a member of theFactoryTalk DirectoryAdministrators group or theWindowsAdministrators group, have that user runFactoryTalk Administration ConsoleorFactoryTalk View Studio, and then help you with your account (for example, reset your password or unlock your account).
Provide Feedback