Do you want to reset the Connector Service
The
Do you want to reset the Connector Service
dialog box appears in one of the following conditions:- Changing the OPC UA Endpoint URL
- Removing an OPC UA Server from a FactoryTalk Linx OPC UA Connector
Select
Yes
or No
in the dialog box to choose whether to reset the FactoryTalk Linx
OPC
UA Connector service. The reset helps ensure FactoryTalk clients get the most up-to-date namespace configuration, but it will stop all service communication and impact the running system.Button | Description |
---|---|
Yes | If changing an OPC UA Endpoint URL:
If removing an OPC UA Server from a FactoryTalk Linx OPC UA Connector:
|
No | If changing an OPC UA Endpoint URL:
If removing an OPC UA Server from a FactoryTalk Linx OPC UA Connector:
|
Provide Feedback