View real-time diagnostics
FactoryTalk Linx
OPC UA Connector provides real-time diagnostic information in two forms:- Diagnostics for a specific OPC UA Server
- Diagnostics for all OPC UA Servers added to the OPC UA Connector
Only a small portion of diagnostic values is included in the
FactoryTalk Linx
OPC UA Connector interface. More detailed real-time diagnostics are available as predefined diagnostic items.To view real-time diagnostics for a specific OPC UA Server
- InFactoryTalk Linx OPC UA Connector, selectOPC UA Servers.
- OnOPC UA Servers, inProperties, scroll down untilDiagnostic Valuesappears.
- (optional) ExpandDiagnostic Valuesif it is collapsed.
To view a summary roll-up of real-time diagnostics for all OPC UA Servers
- InFactoryTalk Linx OPC UA Connector, selectReal Time Diagnostics.
Provide Feedback