Restart the service

Use the Windows Services application to restart the
FactoryTalk Linx
OPC UA Connector service. You can also choose to restart the service when regenerating the certificate.

To restart the service through the Windows Services application

  1. On your computer, select
    Start
    Windows System
    Run
    .
  2. In
    Run
    , enter
    services.msc
    in the box, and then select
    OK
    .
  3. In
    Services
    , right-click
    RnaUaClientDataProviderService
    in the
    Name
    column, and then select
    Restart
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal