Remove an OPC UA Connector
Remove the OPC UA Connector to prevent
FactoryTalk
applications from reading data from the connected OPC UA Servers.Prerequisites
- Obtain the following permissions for the application or area:
- Common > List Children
- Common > Read
- Common > Delete
To remove an OPC UA Connector
- InFactoryTalk Administration ConsoleExplorer, right-click aFactoryTalk LinxOPCUA Connector, and then selectDelete.
Provide Feedback