Data from FactoryTalk Diagnostics Counter Monitor
FactoryTalk Resource and Status server gets FactoryTalk Diagnostics Counter Monitor data from:
- FactoryTalk Linx
- FactoryTalk Linx Instance02
- FactoryTalk Linx Gateway OPC UA Server
- FactoryTalk Linx Gateway OPC DA Server
- FactoryTalk Linx Gateway RTD Server
- FactoryTalk Linx Gateway DDE Server
- FactoryTalk Linx Gateway MQTT
TIP:
FactoryTalk Linx and the FactoryTalk Linx OPC UA Connector also provide diagnostic information as predefined tags associated with a data source they are configured to interface with.
Provide Feedback