Add process dialog

The following are the settings on the
Add Process
dialog.
Setting
Description
Add from Task Manager
Uses this option to select processes monitored by the Windows Task Manager. It is only available for the local host.
Add by process name
Uses this option to add processes by entering the process name manually.
Refresh
Gets the latest data from the Windows Task Manager. It is available for the
Add from Task Manager
method.
Search
Searches a process from the Windows Task Manager. It is available for the
Add from Task Manager
method.
New
Select this button to add a process manually. It is available for the
Add by process name
method.
Process Name
Shows the process name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal