Delete a device address

Delete one or multiple device addresses when you don't want to monitor.
  1. On the
    Device Status
    tab, select the device addresses that you want to delete.
  2. Select
    Delete
    .
    Select
    Yes
    when the
    Confirm
    dialog prompts.
  3. Select
    Apply
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal