Change DEP settings
The DEP settings determine which applications and components are covered by DEP protection. On computers with the necessary hardware capabilities, hardware-supported DEP features are enabled for the same set of applications and components as the software DEP features.
To change DEP settings
- Login in as an administrator of the computer to change these settings.
- Navigate toControl Panel > System > Advanced > Performance Settings > Data Execution Prevention.
- Select one of the following two options:
- Turn on DEP for essential Windows programs and services onlyThis option corresponds to theOptInsetting.
- Turn on DEP for all programs and services except those I selectThis option corresponds to theOptOutsetting.
- Restart your computer so that the DEP setting changes take effect.
Provide Feedback