Disable CIP Security in FactoryTalk Administration Console
If
CIP Security
is disabled, FactoryTalk Linx
will not listen on TCP port 2221.To disable
CIP Security
- Open.FactoryTalk Administration Console
- In theExplorerpane, under theCommunicationstab, right-click the device at the root, and then selectProperties.
- In theDevice Propertiesdialog, on thetab, selectCIP SecurityDisable, and then selectCIP Security(Port 2221)Yes.
- SelectApply.
Provide Feedback