Delete a driver from RSLinx Classic
Follow the steps below to remove a driver configured in
RSLinx Classic
To delete a driver configured in
RSLinx Classic
- OpenRSLinx Classicand clickCommunications > Configure Drivers.
- From theConfigure Driversdialog box, select the appropriate driver from the Configured Drivers list, and clickDelete. The driver no longer appears in the Configured Drivers list.
- ClickView > Optionsand clear theAccept UDP Messages on Ethernet Portcheck box.IMPORTANT:Keep in mind that clearing this check box inRSLinx Classicdeactivates the Gateway Server inRSLinx Classic. You are also disablingRSLinx Classicfrom receiving unsolicited packets across Ethernet.
- Exit and restartRSLinx Classic.
Provide Feedback