Breadcrumb navigation
Use these methods to navigate a hierarchy through breadcrumbs.
To do this: | Do this: |
---|---|
Access a level. | Click any level except the last. |
Return to the highest level of the hierarchy. | Click Home ![]() |
Open a list of sub-levels. | Click the single arrow ![]() |
Return to a recently navigated path. | Click the double arrow ![]() ![]() |
TIP:
If a breadcrumb is too long to fit in the window, the window displays a double arrow. A double arrow indicates there is more content to the left or to the right of the current location in the breadcrumb.
Provide Feedback