Offline devices

Starting from
FactoryTalk Linx
version 6.30, the offline devices will be shown. The Offline devices icon icon to the left of the device indicates this device is offline.
To remove one offline device, right-click the device, and then select
Delete
.
To remove the current offline devices listed in the driver, right-click the driver, and then select
Remove Offline Devices
.
To remove offline devices automatically every time after browsing devices, right-click the driver, and then select
Driver Configuration
>
Advanced
>
Tuning
>
Auto remove offline devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal