Do I need to do anything regarding my device shortcuts after I restore a FactoryTalk Directory or .apa file?
If you restore a
FactoryTalk Directory
using the Restore
option (FactoryTalk Administration Console
or FactoryTalk View
) and/or restore an .apa file (FactoryTalk View SE
Stand-alone or FactoryTalk View ME
), you must manually review and verify the configuration to ensure that shortcuts contained in that directory or application file point to the intended physical devices.Provide Feedback