How do I open FactoryTalk Linx Redundancy Module Configuration Tool?
FactoryTalk Linx
Redundancy Module Configuration Tool is a separate executable
program designed for online operations and configuration of 1756 ControlLogix
Redundancy Modules, including 1756-RM2 and 1756-RM3. A
version of this software is installed with FactoryTalk Linx
. However, the Rockwell Automation
Product Compatibility and Download Center (PCDC) may offer a
newer version.
TIP:
Access to the tool is controlled by
FactoryTalk Security
. You must have the
Open Device Configuration
permission to access the tool.To configure the
Open Device Configuration
permission, open FactoryTalk Administration Console
, and then go to System > Policies > Product Policies
> FactoryTalk Linx > Feature Security
.To launch
FactoryTalk Linx
Redundancy Module Configuration Tool, locate a 1756 ControlLogix Redundancy Module in the FactoryTalk Linx
Network Browser topology view, right-click the module, and then select Device Configuration
.Provide Feedback