When using FactoryTalk Linx to browse a network, some devices appear but are not accessible to the device's information.
When I browse a network using
FactoryTalk Linx
, some devices appear in the browser but I am unable to access the device's information or navigate through the device to display the topology behind the device.When a device and the
FactoryTalk Linx
server are not configured in the same CIP Security zone with FactoryTalk Policy Manager
, this happens. Access the device using the FactoryTalk Linx
server configured in the same zone with the device or add the referenced FactoryTalk Linx
server into the FactoryTalk Policy Manager
zone with the device.Provide Feedback