Add a rack
Racks are locations on the PLC or device type. They determine the addresses you can give to tags or expressions. The available rack numbers are determined by your scanner configuration.
To add a rack to your remote I/O (RIO) scanner
- From theCommunication Setupeditor,right-clickon the RIO scanner and clickConfigure RIOto open theRIO Configurationdialog box. When it opens for the first time, the only element present is the RIO scanner.
- Right-clickthe RIO scanner and then clickAdd Rackto display theRack Propertiesdialog box.Note that adding a rack also adds a group to the tree.
- Select aRack #from the list. The available rack numbers are determined by the scanner configuration.TIP:Each remote module must be assigned a unique rack number and cannot overlap.
- Select aModule Grouping. Module groups are fractions of Remote I/O racks. A full rack consists of 8 module groups. Therefore, each quarter rack consists of 2 module groups. To assign partial racks to a Remote I/O application, set the appropriate module grouping from the list.
- Choose whether the terminal can read only, or both read and write to the rack's I/O space.ChooseFull (Read/Write) access(the default mode) to allow the rack to read discrete Output data from, and write discrete data to, the scanner.ChooseListen Only accessto set the rack to only monitor the data sent to, or returned from, another rack.
- When you are finished adding module groupings, clickOKto close the Rack Properties dialog box.
Provide Feedback