General tab settings
The following are the settings on the dialog box.
General
tab on the FactoryTalk Linx
Server PropertiesSetting | Description |
---|---|
Name | Shows the server name FactoryTalk Linx . This name cannot be changed after the server is created and cannot include dashes or hyphens (–). |
Description | Enter a description for the FactoryTalk Linx server. For example, use this box to describe a component's location, to identify a contact person or number in the event of failure, or to keep track of changes or version information. |
Computer hosting the FactoryTalk Linx server | For local applications, this field shows the name localhost as the computer hosting the FactoryTalk Linx server. This indicates that the FactoryTalk Linx server will execute on the local machine. Because you are configuring a local application, this property cannot be changed.For network applications, this field shows the computer name of the local machine. If you do not want the FactoryTalk Linx server hosted on the local machine, enter a different computer name, or Browse for another computer. |
Server Type | There are two FactoryTalk Linx data servers: instance01 and instance02. Instance01 is the base server which supports all the functions of FactoryTalk Linx . Instance02 is designed to allow applications to have more tags, data clients (for example, HMI clients), and/or controllers without affecting instance01. For more information about the FactoryTalk Linx instance02 service, see What's FactoryTalk Linx instance02 server? |
Provide Feedback