The Run Alarm Command button is missing at runtime
Select the
Run Alarm Command
check box on the Status Bar
tab to display the Run Alarm Command button in the status bar at runtime. If the Run Alarm Command button appears in the status bar but is disabled, this might be because no alarm command is defined.To fix this problem, open the
General
tab in the Alarm and Event Banner Properties dialog box, and then type a command in the Alarm and Event Summary command box. For assistance in creating a command, click the Browse
button, and then use the Command Wizard
.Provide Feedback