I cannot perform actions in the alarm banner
If you cannot click buttons in the status bar, or if double-clicking an alarm has no effect, the Alarm and Event Banner might be running in read-only mode.
For details about using read-only mode with the
FactoryTalk View
SE display client see Help
in FactoryTalk View
.Provide Feedback