SQL Server Express
FactoryTalk Alarms and Events
uses SQL Server
as the database engine for logging alarm and event data.- If you do not have or do not wish to use an existingSQL Serverdatabase, you can installSQL Server2022 Express with the correct features enabled.
- If you already haveSQL Serverinstalled, you can configure the database to log alarm and event log information. Follow the configuration instructions in the, in the section titled "Using an existingFactoryTalk Alarms and EventsSystem Configuration GuideSQL Serverdatabase."
The database can be installed on the same computer used to host other
FactoryTalk
servers or it can be on a separate computer. Depending on the size of your system, you might choose to use a separate computer as a dedicated logging computer to offload processing power.Provide Feedback