ShowAlarmStatus method (AlarmSummary object)
The
Alarm Status Explorer
is displayed. Operators can use the Alarm Status Explorer
to enable or disable alarms.Syntax
object
.ShowAlarmStatus
where
object
—
the name of an AlarmEventSummary object.Provide Feedback