RunAlarmCommand method (AlarmSummary object)
Runs the alarm command that is associated with the selected alarm. Specify the command associated with the alarm in the alarm properties dialog box when configuring the alarm.
Syntax
object
.RunAlarmCommand
where
object
—
the name of an AlarmEventSummary object.Provide Feedback