EventClick event
Event occurs when a user clicks an event row.
Syntax
object
_EventClick
(Item
as EventItem
)where
object
—
is the name of the AlarmEventSummary object or AlarmEventBanner object.Item
—
the event returns an EventItem object, providing access to the field values associated with the selected event row.Example
MsgBox "Clicked on: " & Item.GetColumnValue("EventSource")
Provide Feedback