Use the Alarm Status Explorer at runtime
Use the Alarm Status Explorer to browse for areas, and then for the alarm sources within those areas. Areas subdivide and organize a distributed network application into logical or physical divisions. For example, separate areas might correspond with separate manufacturing lines in a facility, separate plants in different geographical locations, or different manufacturing processes.
Areas are not available with local station applications.
Once you have found the alarm sources you want, you can view their status, or select an alarm and then view details about it.
Provide Feedback