Alarm Status Explorer object model

The
Alarm Status Explorer
displays the
FactoryTalk Directory
area model and the alarm sources contained within that area model.
Operators use the
Alarm Status Explorer
to view and change the status of alarms in the
FactoryTalk Alarms and Events
system. Operators can:
  • Enable or disable alarms.
  • Suppress or unsuppress alarms.
  • Enter comments when enabling, disabling, suppressing, or unsuppressing alarms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal