Status bar in the Alarm and Event Summary

The status bar at the bottom of the Alarm and Event Summary gives and overview of the status of the alarm and event servers in the subscribed-to areas. For the connection status indicators, pointing to the icon will display a tooltip that lists the server names included in the subscribed-to areas and their connection status.
The following table provides a reference to the status indicator icons:
Icon
Description
FTAeAlarmServerConnectionGood
The connection to all alarm and event servers is good.
FTAeAlarmServerConnectionBad
The connection to one or more alarm and event servers has been lost.
FTAeStatusPanelAlarmCount
The number of events in the event list. The text
Event Limit Exceeded
is displayed in this panel if the number of event entries in the Alarm and Event Summary queue has exceeded 2000. The text
Refresh event list
is displayed in this panel when the number of event entries in the Alarm and Event Summary queue has dropped below 2000.
FTAE_InAlarmUnackPanel
The number of In Alarm and Unacknowledged alarms. When the count is zero the icon is gray.
FTAE_InAlarmAckPanel
The number of In Alarm and Acknowledged alarms. When the count is zero the icon is gray.
FTAE_NormalUnackPanel
The number of Normal and Unacknowledged alarms. When the count is zero the icon is gray.
FTAE_ActiveEventIcon
The total number of events that have the status of Active. When the count of events is zero the icon is gray.
FTAE_AlarmFaultPanel
The number of faults for all alarms or the text
Alarm Fault Limit Exceeded
when the number of faults exceeds 500. Double-click the panel to open the
Alarm Faults
dialog box. When the count is zero the icon is gray.
FTAeFilteredNotFilterPanelSummary
The name of the filter used to specify which events are displayed in the events list or the text
Not Filtered
when there is no filter selected.
FTAeSortedPanelSummary
The sort order of events in the event list or the text
Not Sorted
.
FTAE_UnknownMessages
The number of unknown alarm messages that are ignored. When the count is zero, the icon is not displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal