Alarm and Event Log Viewer Properties - States tab

How do I open the Alarm and Event Log Viewer Properties dialog box?
To open the
FactoryTalk Alarm and Event Log Viewer Properties
dialog box at design time:
  1. Open
    FactoryTalk View
    Studio.
  2. Add an
    Alarm and Event Log Viewer
    object to a graphic display.
  3. Right-click the Alarm and Event Log Viewer object and then click
    Properties
    .
Use the
States
tab in the
Alarm and Event Log Viewer Properties
dialog box to configure the runtime appearance of alarms and events displayed in the Alarm and Event Log Viewer.
Use this tab to create a visual meaning for different alarm state and alarm priorities to help the operator decide which events need the most immediate attention. When choosing colors, choose colors that provide good contrast, such as black text on a white background. Avoid low-contrast combinations such as blue text on a black background, or vice versa. Colors are not seen by all people equally. Do not rely on differences in color alone to establish meaning.
The following table provides details about the settings on the
States
tab and how they can be used:
Column
Description
Priority - Urgent, High, Medium, Low, Event
Identifies the priority of the alarm.
This information is read-only.
Text
The color for the message text of the alarm or event.
Click the color box and select the text color.
Background
The color of the background on which the message text of the alarm or event is displayed.
This setting does not affect the background color of the alarm list.
Click the color box and select the background color.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal