AlarmEventLogViewer object

The AlarmEventLogViewer object represents an instance of the Alarm and Event Log Viewer. The AlarmEventLogViewer object is accessible from the container hosting the object.
The AlarmEventLogViewer object contains no methods.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal