Example: Audit messages

If the setting
Audit changes to configuration and control system
is enabled in
Audit Policy
, audit messages are generated when any configuration and control system changes occur across the
FactoryTalk
system.
Examples of messages for adding and removing control system components:
  • Added area [Line2] to application [Network/Paper Mill]
  • Removed area [Line1b] from application [Network/PaperMill]
  • Added graphic display [Overview] to area [Network/Paper Mill/Line2]
  • Removed user [BBilly] from directory [Network/System]
  • Downloaded project [PASTEURIZE] to processor [/NetworkPath/Line1]
  • Inserted rung [XIC B3/0 OTE B3/0] in processor [XYZ/File 2/Rung 10]
Examples of messages for modifying control system values:
  • Modified properties of user [JSmith] in directory [Network/System]
  • Modified properties of server [Line2HMI] in application [Network/Paper Mill]
  • Forced I/O [I1:2/15] in processor [TABLET10] from [OFF] to [ON]
  • Changed security policy [Enforce password history] in directory [Network/System] from [0] to [5]
  • Changed value of tag [HighPressureLimit] in processor [TABLET10] from [100] to [125]
  • Changed value of tag [MaxFeederSpeed] in area [Network/Paper Mill/Line1] from [200] to [300]
  • Changed name of graphic display [Line1Overview] in area [Network/Paper Mill/Line2] from [Line1Overview] to [Line2Overview]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal