Audit Policy Properties
How do I open Audit Policy Properties?
- StartFactoryTalk Administration ConsoleorFactoryTalk View Studioand log on to theFactoryTalkNetwork Directory orFactoryTalkLocal Directory.
- InExplorer, expand theSystemfolder >Policies>System Policies.
- SelectAudit Policy.
Use
Audit Policy Properties
to specify what security-related information is recorded while the system is being used. Audit policies include whether access checks are audited, whether access grants, denies, or both are audited, and so on. Audit messages are sent to FactoryTalk Diagnostics
, where they can be viewed using the FactoryTalk Diagnostics
Viewer. Use these settings to specify what information is audited by the FactoryTalk
system.Setting | Description |
---|---|
Audit changes to configuration and control system | Determines whether to generate audit messages when configuration and control system changes occur across the FactoryTalk system.Default : EnabledTo disable audit logging, set this policy to Disabled .If this policy is disabled, audit messages are not routed to FactoryTalk Diagnostics log files, even if logging destinations are configured for audit messages on the Message Routing tab in Diagnostics Setup .Any changes made to the value of the Audit changes to configuration and control system policy itself are always recorded, regardless of whether audit logging is enabled or disabled. If enabled, audit information is sent to FactoryTalk Diagnostics . |
Audit security access failures | Determines whether to generate an audit message when a user attempts an action and is denied access to the secured object or feature because of insufficient security permissions. Default : DisabledTo record audit messages when users fail to access objects because of insufficient security permissions, set this policy to Enabled . If enabled, audit information is sent to FactoryTalk Diagnostics . |
Audit security access successes | Determines whether to generate an audit message when a user attempts an action and is granted access to the secured object or feature because the user has the required security permissions. Default : DisabledTo record audit messages when users succeed in accessing objects because of sufficient security permissions, set this policy to Enabled . When enabled, this policy might generate a large number of audit messages. Enable this policy only if there is a specific reason for doing so, for example, testing or troubleshooting whether users can access particular features or objects in the system.If enabled, audit information is sent to FactoryTalk Diagnostics . |
Provide Feedback