Restore
How do I open Restore?
- In theExplorerwindow, verify that the applications located in the directory that you are restoring into are not currently expanded or being used by some other product or component.
- Right-clickNetworkorLocal,and clickRestore.
Use
Restore
to specify the name of the backup file to use to restore all or part of a FactoryTalk Directory
.Select one of these archive types:
- A fullFactoryTalk Directorybackup archive. This will be named with its security authority identifier (for example,Network - 72CE2C2E-5175-4C26-98AE-3ABE5AC7F8EC.bakorLocal - C565C77A-4664-4E6C-9779-1EC729B3A8A0.bak). It contains all applications, and all user and computer accounts and groups, passwords, policy settings, and security settings.
- A System folder archive. A System folder archive contains a backup of a System folder, including user and computer accounts and groups, passwords, policy settings, and security settings. It is namedSystem.bakby default.
- An application archive. This archive contains a backup of the application and may contain a backup of the System folder. By default, an application archive file has the same name as the application.
Before restoring an archive file, shut down all
FactoryTalk
software products, components, and services, except FactoryTalk Administration Console
and FactoryTalk
Help, then create a backup archive of the target directory before continuing with the restore process.An archive file created under
FactoryTalk Automation Platform
2.00 (CPR 7) and restored into a FactoryTalk Directory
that has been upgraded to FactoryTalk Services Platform
2.10 (CPR 9) or later automatically updates the data in the System
folder to be compatible with FactoryTalk Services Platform
2.10 or later, while leaving the original data unchanged.
IMPORTANT:
- Do not restore an archive file created underFactoryTalk Services Platform2.10 (CPR 9) or later into aFactoryTalk Directorythat is runningFactoryTalk Automation Platform2.00 (CPR 7). This restore scenario is not supported and may have unexpected results.
- An archive file created usingFactoryTalk Services Platform6.10 cannot be restored on a computer running an earlier version ofFactoryTalk Services Platform.
- Archive files created usingFactoryTalk Services Platform2.90 or later can be restored on a computer runningFactoryTalk Services Platform6.10.
Provide Feedback