Restore Backup File
Use
Restore Backup File
to enter the passphrase which was used during the archive file backup operation. The archive file cannot be restored without the correct passphrase.The passphrase must meet the following requirements:
- Any alphanumeric character or other characters
- Minimum length: 0
- Maximum length: 64
An error message opens if the passphrase you entered is not correct. Enter the passphrase again. If the wrong passphrase is entered three times,
Restore Backup File
closes. Select the archive file and try again.Provide Feedback