Windows-linked user accounts

Windows
-linked user accounts are managed by
Windows
. When accessing
FactoryTalk
resources using a
Windows
-linked account
,
FactoryTalk Directory
relies on
Windows
to determine whether the user's name and password are valid, and whether the account is enabled or locked out. Adding
Windows
-linked user accounts to
FactoryTalk Security
user groups is possible. This allows
FactoryTalk Directory
to determine a
Windows
-linked user's level of access to the
FactoryTalk
system independently of the user's level of access to a
Windows
domain.
Add user accounts to the
FactoryTalk
network directory or local directory from the list of users or groups in a
Windows
domain or workgroup. The
Windows
-linked user accounts in the network directory are separate from the
Windows
-linked user accounts in the local directory.
If the computer is disconnected from the
Windows
domain, the computer must reconnect to the domain before adding
Windows
-linked user accounts. However, any users who previously logged on to the
Windows
domain from that computer can log on to
FactoryTalk
using their
Windows
-linked user account while the computer is disconnected from the
Windows
domain.
If possible, use
Windows
-linked group accounts rather than
Windows
-linked user accounts. When deploying the applications from one domain to another, move the user accounts in a
Windows
-linked user group
from one domain to another by changing the domain to which the group belongs. This allows moving the applications to a different domain without changing or recreating each user account separately, and without recreating all security permissions for the accounts. If the domain an individual
Windows
-linked user account belongs to changes, delete the old account, create the new account, and then recreate the security permissions for the new account.
Use a password for all
Windows
-linked accounts, otherwise intermittent security failures or an inability to log on may occur. Good security practice dictates not using blank passwords with accounts. If not using a password for
Windows
-linked accounts, on your local computer disable the
Windows
local security policy.
Accounts: Limit local account use of blank passwords to console logon only
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal