Status icons

Use these icons to get a quick overview of the status of a data item in
FactoryTalk Live Data Test Client
.
Icon
Description
FTDC_active
The data item is active, and the data item receives updated values automatically as they change at the data server. This is referred to as a subscription value, and is shown in the
Sub Value
column. Changes are displayed at the
Update Rate
for the group.
FTDC_inactive
The data item is inactive. Obtain an updated value for the data item by reading the value of the data item manually, either synchronously or asynchronously. Asynchronous reads return the value at the data server's discretion. Continue reading other values while the
FactoryTalk Live Data Test Client
waits to receive the requested value. The value of a data item requested manually is shown in the
Current Value
column.
FTDC_group_inactive
The group of data items is inactive. Obtain updated values for data items in the group by selecting them and then reading the value of the data items manually.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal