Options
How do I open Options?
- From theFactoryTalk Live Data Test Clientmenu, selectData>Options.
Use
Options
to change the main display update rate or the HMI Emulation Rate of the FactoryTalk Live Data Test Client
.Item | Description |
---|---|
Screen Update Rate (mSec) | The rate, in milliseconds, at which the FactoryTalk Live Data Test Client updates data item values.The current rate at which the data server updates the value of the data item is displayed in the test client in the Updates (/Sec) column. If the data server is sending data faster than the screen update rate, some changes to data items are not displayed. If the data server is sending data slower than the screen update rate, the FactoryTalk Live Data Test Client might be generating unnecessary traffic on the network. |
HMI Emulation Rate (Sec) | The rate, in seconds, at which the FactoryTalk Live Data Test Client switches between groups of data items. |
Provide Feedback