Change the HMI Emulation update rate

Change the HMI Emulation update rate to increase or decrease the rate at which the
FactoryTalk Live Data Test Client
switches between data groups.
To change the HMI Emulation update rate
  1. On the
    Data
    menu, select
    Options
    .
  2. In the
    HMI Emulation Rate
    box, type the number of seconds after which the
    FactoryTalk Live Data Test Client
    should switch to the next group of data items.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal