View data item properties

Due to limited horizontal space in
FactoryTalk Live Data Test Client
, all data item properties may not be visible. Use
Item Properties
to view all properties associated with a data item.
TIP:
When viewing item properties, the number in parentheses is an internal identifier for the data item. Numbers below 5000 are defined by the
OPC
foundation. Numbers above 5000 are vendor-specific.
To view data item properties
  1. In
    FactoryTalk Live Data Test Client
    , select the data item.
  2. Select
    Item Properties
    on the toolbar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal