Read data from the cache
Read data from the cache to show data item values from the local cache instead of devices.
IMPORTANT:
Device Read cannot be set for a specific data item or group; the setting affects all data shown in the
FactoryTalk Live Data Test Client
.To read data from the cache
- InFactoryTalk Live Data Test Client, select any data item.
- SelectData>Device Read.The checkmark disappears, indicating that data is being read from the cache.
Provide Feedback